STEVAL-USBC2DP with USB-C Receptacle
Hi, we were looking at eval board STEVAL-USBC2D to help with designing a USB-C to eDP bridge, but we need this with a USB-C receptacle, is this possible, and how would it be possible?
Hi, we were looking at eval board STEVAL-USBC2D to help with designing a USB-C to eDP bridge, but we need this with a USB-C receptacle, is this possible, and how would it be possible?
Hello everyone,Please I'm designing a new product and I choosed to use the driver ILI9341 for a 2.8" screen.Now I would like to know if there are some minimal performance of the MCU because I wanted to use the STM32F030C6T6TR. Will it work correctly ...
Hello everybodyI'm using a custom board in which there's a STM32F030 that communicate with SPBTLE_RF0 module. With X-CUBE I generate software using X-CUBE-BLE2.2.0.0.I can reset the chip and read response (vendor specific event), but when I try to co...
i use stm32f030 with bluenrg-1 on a card i made i want to test and communicate with it using the BlueNRG GUI --------------------------------------------------------------------------------------------------------------------------But I have problems...
Hello,I'm using a STPM32 to measure the ac line voltage and current. It is connected via a galvanic isolator ISO7341CDW to a STM32F072 with SPI. Most of the time, this works just fine. I can read the correct RMS values for I1 and V1 (Register DSP_REG...
Some context, I'm using a RS485 data line in half-duplex mode to communicate between an STM32F107 (the master card here) and an STM32F072 (the slave card). My end goal is to be able to use the bootloader on the slave card and reprogram it from the ma...
Hi!I have a STM32F765ZITx as master and a STM32F051C8Tx board as slave that im trying to communicated with each other over IrDa. The master is sending 6 bytes (2 startbytes, 1 length of data byte, 1 databyte, 2 checksum bytes) to the slave, which wor...
I'm setting up a MCU to control a stepper motor. I'm aiming to control the stepper motor driver (AMIS-30543) over SPI. My current goal is to get the driver to respond to my SPI commands so I know it's correctly receiving my commands. The driver respo...
I have hade issues now for 8 month, I cant connect to the stusb4500 chip i have on my custom board for PD profile programming, The gui always tells me there is no board connected and the HW checker wont find anything. I can connect to the f0732 with ...