Interface and connectivity ICs

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

st7789h2 LCD MODULE issues

hello sir,My self-Mahesh firmware engineer Currently I am working with 1.54 inch display module(st7789h2),This module is configured with four wire SPI.I am facing some issues 1, Pixel writing is very slow. 2, Not able to control the brightness. 3, I...

MRedd.3 by Associate II
  • 1619 Views
  • 11 replies
  • 0 kudos

Tutorial code for FMC interface with LCD TFT fails on my device, I got it to run by editing the code but the graphics updates are notably slow. Am I misunderstanding how FMC on STM operates entirely?

I was following a video tutorial for F(S)MC setup for an 8080 LCD interface. I have an Elegoo ILI9341 shield. When I ran the code, my display was just a flashing white background no matter what functions I tried to call.All of the tutorial functions ...

NNagy.1 by Senior
  • 412 Views
  • 0 replies
  • 0 kudos