Interface and connectivity ICs

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VD6283TX ALS not working properly

Hi ,I am working on STM32L0 series controller with VD6283TX ALS on I2C interface.Though code is available for the sensor, my requirement is to write own code that will control the sensor. Sometimes it reads the RAW data from sensor and sometimes it ...

BChav.1 by Associate III
  • 426 Views
  • 3 replies
  • 0 kudos

how to set custom frequency for st7580 ?

Hi I am using NUCLEO-L053R8 with XNUCLEO- PLM01A1 board connected which is having ST7580. i am able to run the basic example given but now i wanted to change the Maximum central frequency which is in configurable as per the document *https://www.st.c...

0693W00000HpYlCQAV.png 0693W00000HpYoKQAV.png
ytriv.1 by Associate
  • 243 Views
  • 0 replies
  • 0 kudos

Resolved! Lora node ns1 AT master

Hi everyone, I have a p-nucleo lorawan 3 kit with a nucleo-l073rz board and a lorawan ns1 lora board. ​I'm trying to setup the AT master example from I-NUCLEO-LRWAN addon using keil uvision. I uploaded the program and activated the CMD_DEBUG but I do...

PDevo.1 by Associate II
  • 469 Views
  • 4 replies
  • 0 kudos