Interface and connectivity ICs

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STUSB4710: Default Configuration Confirmation

Hello,I apologize if the answer is obvious but I want to confirm my understanding for the STUSB4710 (USB-C PD controller). Section 4.1 of the datasheet mentions that the default values for the voltage and current settings, which require NO I2C progra...

0693W00000Y9dfbQAB.png
KMew by Senior III
  • 438 Views
  • 3 replies
  • 0 kudos

VBUS monitoring not working on STUSB1602

Hi guys ! I am trying to implement a USB-C powering and communication between 2 of my devices. There is no Power Negociation implemented yet. The default voltage is 5V.I want to make sure my source device is safe so I would like it to shut down VBUS ...

0693W00000QOOZCQA5.png
VSpad.1 by Associate II
  • 251 Views
  • 1 replies
  • 0 kudos

Resolved! STUSB4700/4710 I2C register details

I am working on a project using a few STUSB4710 and some STM32F0 family microcontrollers. I am looking for details about the registers of the STUSB4710. In the datasheet I can find only the I2C register map and the details of the PDO registers but no...

Setting up STUSB4500 sink for 12V,5 A

We are using the STUSB4500 PD chip in one of our applications. The requirement is to set the Power delivery to 12 V and 5A for the sink. I have been referring the driver code provided by ST to program our microcontroller. To set PDO to 12 V and 5 A, ...

ARadh.1 by Associate III
  • 1050 Views
  • 18 replies
  • 0 kudos