Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! BLE : Cannot enable notification on the client characteristic configuration descriptor (0x2902)

Hello,i defined a characteristic with notify propriety :  ret = aci_gatt_add_char(Service2_Handle1,UUID_TYPE_128,&char_uuid,26,CHAR_PROP_NOTIFY | CHAR_PROP_WRITE | CHAR_PROP_WRITE_WITHOUT_RESP,ATTR_PERMISSION_NONE,GATT_NOTIFY_ATTRIBUTE_WRITE | GATT_N...

malarab by Senior II
  • 2499 Views
  • 2 replies
  • 0 kudos

VL53L1X People count

Dear SupporterWe make a design using the "VL53L1X" for people counting applications.To test it, we placed it above the entrance of a room (as in the YouTube link "People Counting Using a Single ST Time-of-Flight Sensor" posted by ST Microelectronics)...

Beacon discovery problem

Hello,I have configured the BLE Beacon V1.0 sensor with the Nano Beacon software, I can detect it with applications like nrf Connect or ST BLE Toolbox. I've programmed a stm32 card as a client, I can detect the devices, but I can't detect the beacon ...

AMACH1_5-1692876253934.jpeg AMACH1_6-1692876261444.jpeg AMACH1_7-1692876501396.png AMACH1_8-1692876580965.png
AMACH.1 by Associate II
  • 853 Views
  • 0 replies
  • 0 kudos

STW81300 PLL Low power at 2.4GHz

Hi all I am using the STW81300 for a project and the Pout level makes sense for 8-16GHz port.  When I set the frequency to 2.4GHz, I am getting only -15dBm or so, while the second and third harmonic of this at 4.8GHz and 7.2GHz are 8dB higher in powe...

mohsenz by Associate
  • 1087 Views
  • 0 replies
  • 0 kudos