Interface and connectivity ICs

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Heart beat signal.

Hi, MURALI SELVAM from India. I using "STM32H743VIT6" I want know heart beat signal hardware configuration, in the project I using three MCU for safety purpose, in case 1st MCU will get failure, 2nd one is take control, 2nd one will get  failure, 3rd...

murali by Associate III
  • 247 Views
  • 9 replies
  • 0 kudos

HOW TO Calculate TIM5 AND TIM6 PERIOD

/////////////////////////////////////////////TIMER 5 /////////////////////////////////////void MX_TIM5_Init(void){TIM_ClockConfigTypeDef sClockSourceConfig = {0};TIM_MasterConfigTypeDef sMasterConfig = {0};htim5.Instance = TIM5;htim5.Init.Prescaler =...

SITARAM by Associate II
  • 110 Views
  • 2 replies
  • 1 kudos

HAL i2c 0x78 problem

iam using nucleo f446re for reading from and writing to i2c eeprom on arduino i used to extrat the 7bit address from the 10 bit using this core for that void writeLexChip(uint16_t TenBits_slave_address, uint8_t firstRegisterByte, uint8_t secondRegist...

RTC: Oscillator Fail detection.

Hi All,I am currently using your RTC: M41T81M6F and I am evaluating to add, as additional homologation, your RTC: M41T81SM6F.I have seen that the “new” one has additional features such as oscillator Fail detection and Battery Low detection, however o...

AKhar.4 by Associate
  • 124 Views
  • 0 replies
  • 0 kudos

spirit1 instruction

"Using SPIRIT1 to transmit packets. I need an empty command (like NOP). Will it be generated automatically, or do I need to add it manually? I didn't find any relevant explanation in Datasheet. Also, can FEC be manually disabled?"

hsu77777 by Associate
  • 226 Views
  • 0 replies
  • 0 kudos