Interface and connectivity ICs

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Configuring STM32U575 for I2C DMA transfer

I am working through a workshop tutorial on how to configure and use GPDMA transfers via the linked list functionality provided in STM32CUBEMX. When setting the linked list runtime configuration a Source Address, Destination Address and Data size are...

ITayl.1 by Associate
  • 715 Views
  • 0 replies
  • 0 kudos

VD6283TX ALS not working properly

Hi ,I am working on STM32L0 series controller with VD6283TX ALS on I2C interface.Though code is available for the sensor, my requirement is to write own code that will control the sensor. Sometimes it reads the RAW data from sensor and sometimes it ...

BChav.1 by Associate III
  • 700 Views
  • 3 replies
  • 0 kudos

Have you seen the source code to the MFX?

Hi All,Some of the grander Evaluation/Discovery boards use an STM32L152 as a slave Multi Function eXpander with an I2C interface. It's pre-programmed with firmware that provides access to some of the peripherals on the board.As it happens, I'm about ...

DOsbo by Senior
  • 589 Views
  • 1 replies
  • 0 kudos