Interface and connectivity ICs

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

HI, I use DSP28335 to read the rtc M41T94 chip time, the mode is (00 or 11), but the oscilloscope decoding always returns FF or 00. Hope to get your help. thanks ZGH

The DSP28335 processor is used to communicate with the M41T94 real-time clock chip (RTC). The RTC uses SPI for communication. The basic configuration method is to write command + write time, then read command + read time, but the read time is basical...

0693W00000Nq5yqQAB.jpg 0693W00000Nq5zKQAR.jpg 0693W00000Nq5zPQAR.jpg
GZhan.6 by Associate
  • 240 Views
  • 0 replies
  • 0 kudos

RTC M41t62 driver file missing.

Posted on April 06, 2018 at 12:04hello,i am trying to interface RTC M41T62 with nrf52835.i got the driver of RTC. when i trying to put this driver in application i got an object file error. actually this is an header file error. some  definations ar...