Interface and connectivity ICs

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Lora node ns1 AT master

Hi everyone, I have a p-nucleo lorawan 3 kit with a nucleo-l073rz board and a lorawan ns1 lora board. ​I'm trying to setup the AT master example from I-NUCLEO-LRWAN addon using keil uvision. I uploaded the program and activated the CMD_DEBUG but I do...

PDevo.1 by Associate II
  • 456 Views
  • 4 replies
  • 0 kudos

Is there a possibility to power off the Murata Type ABZ module completely, and remember the settings for next power on ? Like for the RN2483 ?

Hello everyone,I use the Murata Type ABZ module as an AT Slave device from a bigger microcontroller. As the Murata module is one among many modules on my board, I have included the possibility to turn it off completely with a load switch. Rather than...

Loïc by Associate II
  • 227 Views
  • 0 replies
  • 0 kudos

Wake up b-l072z-lrwan1 from LoRa

Hello,I have 2 b-l072z-lrwan1 working with the ping-pong application.I intend to change the example, where the board which will receive the PING will start stopped and will turn on only when a radio message is sent (in my test case, the PING).Is it p...