Interface and connectivity ICs

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STUSB1600A and STANDBY_POWER_MODE_DISABLE

Hello,The STUSB1600A has a standby power mode that is described in the datasheet as being disabled by default, and can only being enabled through NVM reprogramming.However, when using the STUSB GUI (v. 3.2.3) connected to a STUSB1600A and NUCLEO-F072...

E4A by Associate
  • 112 Views
  • 0 replies
  • 0 kudos

Dual STUSB4710 Power Management

I am designing a usb type-c charger. I want to use 2 microcontroller and 2 STUSB4710.Type-C Output will be 20V 3.35A 67W.I want to do power management between these USB Type-C outputs.I have questions. Can you please answer them? 1. Are there any I2C...

STUSB1600A can't switch to Source

I have STEVAL-CCC002V1 with STUSB1600A controled with STM32F103 over I2C. Samsung Galaxy Tab connected to USB-C and I want to charge it.But I can't switch to "source power role". No matter how hard I try the controller is still in sink.Here I have a ...

20240131_125212.jpg
riske by Associate II
  • 127 Views
  • 0 replies
  • 0 kudos

L9663

Direct interface of communication interface Is the transceiver directly connected to the PSI5 interface of the ECU

JL1 by Associate II
  • 127 Views
  • 0 replies
  • 0 kudos

L9663

Mode 2 Can read and write sensor data directly through the psi5 operation register?

JL1 by Associate II
  • 105 Views
  • 0 replies
  • 0 kudos