I2C after last update is fail on NUCLEO-G474
I2C after last update is fail on NUCLEO-G474, fail when I write 24LC256 and I2C LCD Display MMCOG21605D6W on the first line has shifted with 4 characters. What can I do to fix it?
I2C after last update is fail on NUCLEO-G474, fail when I write 24LC256 and I2C LCD Display MMCOG21605D6W on the first line has shifted with 4 characters. What can I do to fix it?
WiSE Studio does not connect to Segger J-Link, although Atollic TrueStudio and J-Link Commander do. Could it be in a different driver? Why different?I am evaluating the BlueNRG-2 eval board that is working under TrueStudio (that cannot compile an SDK...
As of version 1.1.0 of X-CUBE-SUBG2, file app_x-cube-subg2.c contains two uninitialized pointers. typedef struct { uint8_t Cmdtag; uint8_t CmdType; uint8_t CmdLen; uint8_t Cmd; uint8_t DataLen; uint8_t* DataBuff; // This pointer }AppliF...
Hi,When I am using the `aci_gatt_update_char_value_ext_IDB05A1` function with the argument `value_length=118` the board goes to `HardFault_Handler`.I am using Nucleo-H743ZI2 with X-NUCLEO-IDB05A1 BLE Expansion board. The code is here at this specifi...
Posted on April 04, 2016 at 10:15Good morning to all, I have a little problem with my module. After a filesystem update I send the command AT+CFUN=1 to reset the module. The module return OK, return ''+WIND:2:Reset'' but don't resect. Why?Stefano ...
Posted on July 27, 2016 at 06:31Hello! I have some troubles with wifi module. At first I have upgraded a firmware of my SPWF01SA.11from ver 3.3 (default) to ver 3.5 following instructions. And since this moment I found unexpected reaction of module...
Posted on April 10, 2015 at 23:08I have been looking at the advertising data delivered to the Central by the BLE_EVT_BLUE_GAP_DEVICE_FOUND event when the Peripheral is in a variety of modes. (1) When I reset the BlueNRG and issue a BLUEHCI_GAP_SET_G...