Interface and connectivity ICs

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

WiSE Studio does not connect to J-Link

WiSE Studio does not connect to Segger J-Link, although Atollic TrueStudio and J-Link Commander do. Could it be in a different driver? Why different?I am evaluating the BlueNRG-2 eval board that is working under TrueStudio (that cannot compile an SDK...

0693W00000QMd9UQAT.png
idolezal by Associate II
  • 872 Views
  • 7 replies
  • 0 kudos

Programming the BlueNRG-1 Over SWD

Posted on June 30, 2017 at 07:37Hi All,I've been working on a project which involves programming a BlueNRG-1 microcontroller over SWD. As recommended far and wide, I have ensured that DIO7 is pulled high and have followed reasonable design practices...

NUCLEO-L476RG/IDB04A1 ITM and SPI

Posted on December 14, 2015 at 12:01Hello,I use a IDB04A1 bluetooth shield on a STM32L476RG Nucleo board and I want to redirect the standard output through the ITM port to see my printf in Keil uVision.The problem is that the SWOTRACE pin of the ITM...

vanson by Associate
  • 264 Views
  • 0 replies
  • 0 kudos