Interface and connectivity ICs

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! lsm303 stm32F407G

I have some following up questions after my last post: https://community.st.com/t5/stm32-mcus-products/lsm303dlhc-c/m-p/597950#M224881. I now have a code that does not give any errors. with the librarys in the picture below. But when i run the code a...

Chris_student_0-1698235852918.png

CubeIDE Error : strange error using git

Hello, I'm using git with my project based on a CubeWL example. After wanting to add this gitignore and delete unnecessary files (i.e. examples that I don't use, but I kept the drivers of course), it doesn't work anymore... ...Git/STM32WL55/STM32Cube...

0693W00000LwxqQQAR.png
LLr.1 by Senior
  • 982 Views
  • 6 replies
  • 0 kudos

STCUBEMX code generation missing some pins?

So I'm new to the stm32 line up and I'm currently trying out the STCUBEMX code generator. After generating the code, I can't seem to find the configurations for the pins I selected. For example, I chose PD5 and PD6 as TX and RX for USART2. But when I...

SYes.1 by Associate
  • 446 Views
  • 1 replies
  • 0 kudos