Interface and connectivity ICs

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

BLUENRG232 i2c communication with eeprom

How can i assign addresses in EEPROM code of BlueNRG 232 for different vaiables location.As in the sample code bluenrg232 only device address is used not the register address where we will save varaible values memory.function taken from sample i2c ...

Pshar.1 by Associate II
  • 275 Views
  • 1 replies
  • 0 kudos

Bluenrg2 eeprom

Hi,I'm trying to interface this eeprom with Bluenrg2 http://ww1.microchip.com/downloads/en/DeviceDoc/Atmel-8828-SEEPROM-AT24CM02-Datasheet.pdfI can write correctly. I can read 1 byte at time correctly. Trying to read more than 1 bytes results in inco...

Resolved! Serial EEPROM Byte and Page Write Endurance

Posted on April 11, 2017 at 11:42Hi There , We are currently working on a project using an EEPROM to store sporadic data. The eeprom is a 24AA512 with 512kbits memory, from Microchip.We use it to store datalogging data from our application. The prob...

eg7963 by Associate III
  • 348 Views
  • 3 replies
  • 0 kudos

M95512-A125 EEPROM IDLE CHECK

Posted on December 09, 2016 at 16:49Hi there! I am using M95512-A125 serial EEPROM in my automotive project. My question is, when i'm going to do some operation on the EEPROM, how do I know if it is completely IDLE? I know that bit WIP in the status...

IDB003V1 EEPROM usage

Posted on December 17, 2014 at 13:38Hello! I write my configuration data to internal EEPROM of CPU. I place my configuration data from the very beginning of EEPROM: at address 0x08080000. If I read EEPROM content immediately after writing then I s...

pbfn46 by Associate
  • 222 Views
  • 0 replies
  • 0 kudos