Hello,is it possible to enable/disable the "readout protection via SWD/JTAG mode for BlueNRG devices? Is it possible with openocd?BR Sebastian
Relating to STUSB4700 / 4710 datasheet I suggest the device address is the same as for 4700 with all adr pins set to 0.But no description in 4761 datasheet for I2C interface or register map.
Hi everyone,I'm confused in regars of BOM for SMPS for BlueNRG-LP. In the Reference Manual we can see the following recommandation: and in the document for the evaluation board there is another solution: Would it be possible to get an answer if both...
Posted on June 27, 2018 at 21:59Unlike the datasheet for BlueNRG-2 (https://www.st.com/resource/en/datasheet/bluenrg-2.pdf ), the BlueNRG-1 datasheet (https://www.st.com/resource/en/datasheet/bluenrg-1.pdf ) lacks chapter bookmarks. I really miss th...
Posted on January 31, 2018 at 13:59Hello,I'm trying create a script in uPython in order to get control of the wifi module SPWF04SA/SC. I have successfully updated FW and FS via UART and right now I'm using RELP via UART to test out some code. Can so...
Posted on October 04, 2017 at 11:31Since I have started to work with SPWF04SA, I have seen lots of mistakes in the documentation (specially about the SPI interface). Hopefully, the community help me but I wonder when the new version of the doc will ...
Posted on November 25, 2014 at 17:00Dear ST The application command interface (ACI )document UM1755 is incomplete. Many of the calls don't list the parameters to pass, and the results returned. In some cases it is possible to find this information f...