Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

[BLUENRG-LP] Scan devices when using CODED_PHY

Hello everyone. I'm facing a issue when I try to use CODED_PHY instead 1M_PHY. When I start a GAP_GENERAL_DISCOVERY_PROC, the stack returns: 0xD1 (BLE_STATUS_INVALID_SCAN_CONFIGURATION).Could anyone help me? The scan configuration is (return 0x00 - O...

LTrin.1 by Associate II
  • 1000 Views
  • 0 replies
  • 0 kudos

LNB Efficiency

Using the STEVAL-LNBH06 I am not able to achieve 93% efficiency as stated in the data sheet. Please advise why this might be.inout voltage: 12Vload: 43ohm power resistor for each channel (draw 420mA per channel)measured input power: 20.4Woutput power...

JAlex2 by Associate
  • 1709 Views
  • 2 replies
  • 0 kudos

NUCLEO-H743ZI2

Hello Everyone!I think it's a weird question, however, I am new to NUCLEO-H743ZI2.  Actually, I am facing the issue of low-speed data transfer from MCU to PC (LabVIEW). Before, I was using programming and debugging USB ports to transfer data to LabVI...

LIN transceiver

Hi team,Is there any transceiver that has 2 channels and is ISO14230 or ISO9141 compatible? The most important is that this transceiver must supports 24 V in VBB pin (vehicle batery). Also is important that there is a level changer internally.

Aarong by Associate
  • 1042 Views
  • 0 replies
  • 0 kudos

L9369 getting voltage from SH1, SH2

Hello. ST team.i'm using L9369's voltage measurement function.i read L9369 manual, and i send below SPI commands(no.0~6) for initial driving.(my purpose is to drive FET : HS1 A, B ON / LS2 A,B ON)00xb5019ff810xb5a15fef20xb720b54d30xb480aa9840x40a0000...

ldong.1 by Associate III
  • 1475 Views
  • 1 replies
  • 0 kudos

LVDS transceiver RHFLVDSR2D2 failure info

Good afternoon, We are evaluating the possible consequence for the LVDS transceiver RHFLVDSR2D2 in case that it is supplied with a voltage above its absolute value which is 4,8V.In particular we are asked to evaluate the case that voltage applied to ...