STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Porting to STM32F429VIT6 from STM32F413H

Porting to STM32F429VIT6 from STM32F413HChanged made so far:1) Choosing the example from the same STM32 family as starting point if possibleSTM32F413H Discovery example chosen: 2) Editing the used IDE configuration files to rename what needs to be re...

Ahmed by Associate III
  • 1900 Views
  • 3 replies
  • 0 kudos

Distro INfluence on security

HelloI am using Buildroot instead of Yocto with STM32MP157C and I wanted to know if there is a difference while parametrizing security features on my MPU and if the community.st.com website is relevant in my case or not.Best regards

STM32F767IG7x+SBSFU

Running USB virtual serial port program separately is normal,but download the virtual serial program through sbsfu, USB can't recognize it.Can you give me some suggestions,thankyou very much.

Skaix.1 by Associate
  • 1457 Views
  • 2 replies
  • 0 kudos

STM32L476RG_NUCLEO_2_Images_SBSFU doesn't build

I'm trying to finish a first homework related to the SBSFU. I can build the SECoreBin project which at the end generates the SECoreBin.bin file. So it works fine. Next I try to build the SBSFU project but then I get "Nothing to build for project STM...

MPyt.1 by Associate
  • 1288 Views
  • 2 replies
  • 0 kudos

Read protection self reset

I'm trying to set read protection on STM32F412 to level 1 via JLink during initial flashing. I'm issuing next commands:J-Link>w4 0x40023C08 0x08192A3B Writing 08192A3B -> 40023C08 J-Link>w4 0x40023C08 0x4C5D6E7F Writing 4C5D6E7F -> 40023C08 J-Link>me...

confucij by Associate II
  • 4252 Views
  • 7 replies
  • 0 kudos