STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 G0 Setting Read Protection With Batch(.bat) File

Hi, I am trying activate read protection to level-1 with using batch(.bat) file. I am commanding to ST- Link Utility via batch file. My batch file code is like that:@ECHO OFF"C:\Program Files (x86)\STMicroelectronics\STM32 ST-LINK Utility\ST-LINK Uti...

SSone.1 by Associate III
  • 2498 Views
  • 2 replies
  • 0 kudos

Homework SBSFU Problems

Make make clean Cannot run program "make": Launching failedError: Program "make" not found in PATHPATH=[C:/ST/STM32CubeIDE_1.4.2/STM32CubeIDE/jre/bin/server;C:/ST/STM32CubeIDE_1.4.2/STM32CubeIDE/jre/bin;C:/ST/STM32CubeIDE_1.4.2/STM32CubeIDE/jre/lib/a...

FBone.2 by Associate
  • 1019 Views
  • 1 replies
  • 0 kudos

Enabling SBSFU security flags cripples my code

I've ported the SBSFU package for my user app. It works great when only read out protection is enabled. Everything works as it supposed to. However, when I activate other security flags random errors/problems arise in the code. For example, when I ac...

MHoss.1 by Associate III
  • 3808 Views
  • 9 replies
  • 0 kudos

How to Debug Code Executing from OctoSPI / OTFDEC in Keil MDK?

Hi guys,I'm currently utilising SBSFU as an external flash secure bootloader (with all security settings turned off for debug) using the STM32H7B3's OTFDEC (On-the-fly Decryption) peripheral.My user application boots and runs via the OFTDEC and memor...

ALowe by Associate II
  • 3183 Views
  • 4 replies
  • 0 kudos

What is de CRC16 used on SPI peripheral? the Polynomial is configurable, but the init value and reverse or not, is not documented.

I have a SPI on STM32F746 configured:/* SPI6 init function */void MX_SPI6_Init(void){ hspi6.Instance = SPI6; hspi6.Init.Mode = SPI_MODE_MASTER; hspi6.Init.Direction = SPI_DIRECTION_2LINES; hspi6.Init.DataSize = SPI_DATASIZE_16BIT; hspi6.Init.CLKPolar...

FMaro.1 by Associate II
  • 1088 Views
  • 1 replies
  • 0 kudos

X-CUBE-SBSFU installation issue inconsistencies

When comparing installation results with contents of Security_WS_Tools_Installation.pdf, there are the following inconsistencies: Running C:\STM32SecuWS\Tools\Other\CheckEnv.bat does not complete, as it requests STM32CubeProgrammer v2.5.0, whereas ST...

rongal by Associate II
  • 2172 Views
  • 4 replies
  • 0 kudos