User Activity

The LPTIMER OF STM32l0(Config BASED ON LSI) can cause the CPU to be temporarily stuck in the LPTIM ISR with no way for the CPU to clear the IRQ.The bug is well described here with a workaround, can someone from ST confirm this issue, and if there is ...
I want to set RDP LEVEL1 TO my based battery device, I followed this link but seems not working https://www.youtube.com/watch?v=f7vs0NwZPFoit always needs a POR to load correctly the OB.anyone has tried this out with stm32L0?
Hello, I would like to set the RDP LEVEL for my stm32l0 MCU without using ST link utility software, to be more specific, how I can set the level in the firmware to be flashed in which area ? and is it possible to add a script to linker to set the ...
Hi community, Is there any one here tried to connect Winc3400 from ATMEL/MICROCHIP to an STM32f4 or any other ST mcu via SPI interface ? any success with refactoring winc3400 driver with ST SPI HAL??.Please advice !thanks.
Hi,According to application note for STM32F4xx protection features ,the reverse from RDP L2 to RDP L1 is not possible due to a JTAG fuse, does this mean also that the MCU can check the fuses before checking the RDP? Is it possible to change the Level...