STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Add CRC value to axe file

Hi all,I'm trying to add the STM CRC32 to the hex or axf file, after this I need to convert it to .bin file because I've a Bootloader and I want to check the CRC32 to see if there's a valid image stored. I'm using srec_cat but doesn't work. Thanks.

SBSFU porting to a custom board!!

Hi there..It will great to have a walk through about porting the SBSFU on a custom boards!!!I followed the instructions in the "Getting Started with SBSFU....." AppNote, but it's not working. I will highly appreciate you for any help.ThanksJitu

JChou.1 by Associate III
  • 3802 Views
  • 7 replies
  • 2 kudos

Running TF-M example application to download tfm_s_enc_sign.bin through ymodem and then decrypt error when secure boot at STM32L562

Dear st team,  I have a development issue when running TFM example application at STM32L562.After download the tfm_s_enc_sign.bin through ymodem,print error log"[ERR] Image in the secondary slot is not valid!" when secure boot .ALL other 3 bin(tfm_s_...

Pxu.1 by Associate
  • 1862 Views
  • 3 replies
  • 0 kudos

Resolved! SBSFU Image 2 F413H errors

When the files are accessed. Some of the symbols are not resolved and shows up as errors, however the project compiles fine. Has anyone else come across this issue?

0693W000005B2tFQAS.png
Ahmed by Associate III
  • 1276 Views
  • 1 replies
  • 0 kudos

Auto-detecting comport scripts doesn't works (fix inside)

Hello, On my setup impossible to run the 2 scripts auto-detecting the COMPORT of the current plugged board. Wrong COMPORT is returned and the Teraterm macro crash.I've patched the original scripts to ask you for the COMPORT. Modified files StartTTPL4...

Phil242 by Associate II
  • 4963 Views
  • 13 replies
  • 1 kudos

DevBoards delivery for 12th of November workshop

I'm registered at the workshop which will take place on 12th of November but I still didn't received any boards, is there a tacking number available or how can I find out if my parcel is still on the way?

AHalm.1 by Associate II
  • 1470 Views
  • 4 replies
  • 0 kudos

Resolved! Is the CRC peripheral used by the FUS services on the STM32WB?

Hi -I had been working on getting FUS support for upgrading images integrated into our firmware, and I discovered that my initialization of the CRC peripheral was causing the FUS subsystem to reject all upgrade attempts. I couldn't find any document...

Tim.N by Associate III
  • 1798 Views
  • 3 replies
  • 0 kudos