STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1740 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4887 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9585 Views
  • 5 replies
  • 3 kudos

Experience in braking/recouperation operation mode?

Hi Based on some discussions in the community about torque problems at low speed I am wondering, if I will run into problems with my application.I would like to use the STEVAL-SPIN3201 board to drive a 48V BLDC motor. It is a start stop application ...

PBlat.1 by Associate
  • 1556 Views
  • 3 replies
  • 0 kudos

Regarding Spikes in Phases in BLDC Controller

Hello All, I'm developing 48Volt 700Watt BLDC Motor Controller Using STM32 Controller. I didn't use STM Motor Control Workbench Tool for this Project. I developed my own library and source code for this project. When motor is running initial spikes i...

0693W000003RUsYQAW.jpg 0693W000003RUsTQAW.jpg

External Interrupt IRQ Handler with ADC DMA IRQ Handler

Hello everyone,I'm trying to build a sensorless 6 step BDLC motor control. I'm using 3 external interrupts to detect rising and falling BEMF signals and 6 step commutation sequence and the motor works fine for different PWM values. Now I'm trying to...

KKuma.4 by Associate
  • 3502 Views
  • 6 replies
  • 1 kudos