STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1729 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4875 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9574 Views
  • 5 replies
  • 3 kudos

ST32Cube can't find MotorControl files?

I am having a devil of a time loading an existing MC_SDK project using STM32Cube. When I try to load an existing project potentiometer.ioc I get an error "Can't Add: Motor Control files not found". Does ST32Cube not see MC_SDK?To be more specific I l...

BTrem.1 by Senior II
  • 1230 Views
  • 1 replies
  • 0 kudos

Stm32 workbench issue

Me and my team have been working for a while now on the Stm32 workbench. The Motor Profiler calculates the parameters for the motor, and are then they are imported to the workbench to generate code to TrueStudio IDE. We are facing some issues with dr...

OTcho.1 by Associate
  • 1337 Views
  • 1 replies
  • 1 kudos

Stop Motor with SDK library

Hello,I'm working with NUCLEO F302R8 + X-NUCLEO IHM08M1.I was wondering if it was possible to stop the motor in a fixed time with the Motor Control SDK library v5.4.4.Thanks for the support,

UVagl.1 by Associate II
  • 1190 Views
  • 1 replies
  • 0 kudos

How to start motor using FOC from zero speed?

Hi all,I am using STM32F303RB with iHM08M1 to control a BLDC motor.I want to startup my motor from zero speed using FOC, but the motor shakes at the beginning.I have tried to increase Vq, but the motor will have a big vibration if Vq is set to high, ...

Alex Chen by Associate II
  • 7819 Views
  • 10 replies
  • 0 kudos