Skip to main content
Associate II
July 10, 2020
Question

Stop Motor with SDK library

  • July 10, 2020
  • 1 reply
  • 628 views

Hello,

I'm working with NUCLEO F302R8 + X-NUCLEO IHM08M1.

I was wondering if it was possible to stop the motor in a fixed time with the Motor Control SDK library v5.4.4.

Thanks for the support,

This topic has been closed for replies.

1 reply

Laurent Ca...
Senior III
June 15, 2021

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards