STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LWIP recompilation

Hello Dear DevelopersI don't know what is the procedure, but when a file is added to the project, the compiler no matter if it is Keil, STM32cubeide, or IAR, does a complete rebuild while LWIP is added to the project. What should I do or What I can d...

Resolved! STM32F446RE USB CDC device problem

Hi, I'm trying to follow this tutorial :- https://youtu.be/Hk--a4K497M -- demonstrating how to transmit simple string to PC via usb virtual com port. Unfortunately, I'm getting no output on my serial port. During debugging, I found that CDC_Transmit_...

0693W000007ZdGGQA0.png
KSriv.1 by Associate
  • 2922 Views
  • 2 replies
  • 0 kudos

Hi I'm using STM32F030R8 and trying to communicate with atecc508a using I2C. The datasheet of atecc508a says that it needs a wake up command by transmitting 0x00 at its I2C address 0xC0.

I use the HAL library function to transmit the wake up command to its I2C address.#define I2C_ADDRESS 0xC0HAL_I2C_Master_Transmit(&hi2c1, I2C_ADDRESS, 0x00, 4, 1000)but my code always return HAL_ERROR and the chip never acknowledges. I'm fairly new t...

BNara.1 by Associate
  • 1450 Views
  • 1 replies
  • 0 kudos

Moving project from 1 processor to another.

Hi I have a project where I have a ST32L433Vx 100 pin 256K memory and 64K ram. I am using a display and as I need a lot of memory I have to upgrade. I am looking for a drop in chip and found the STML452VETx which is 512K and 160K ram. I looked at th...

Serial Bootloader baudrate mismatch

We have a system with STM32L431CCU which gets its initial firmware through serial download (as described in AN3155). We use USART1 and applied pattern 6 as described in AN2606. The software on the host side (embedded linux system) is either stm32fla...

0693W000007ZaYqQAK.png
MW by Associate II
  • 804 Views
  • 0 replies
  • 0 kudos

STM32F427 Reading UART

Hello!I'm doing an application in which my control board is I2C slave of my PC and my control board has to communicate with another board (let's call it test board) via UART.This test board uses custom UART text commands to perform tests on itself.Fo...

BBori.1 by Associate II
  • 1064 Views
  • 1 replies
  • 0 kudos