STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! X-CUBE-CELLULAR Update

I'm working on a project with version 5.2 of X-CUBE-CELLULAR and there is an new version 6.0. I tried to download it and use it to update my project but I see that folders structure is not the same, thus updating my project is difficult. What is the ...

NCatt.1 by Associate III
  • 2433 Views
  • 5 replies
  • 0 kudos

Resolved! (Solved) Change BG96 modem configuration

Hello everyone, I'm working on a project that I did not create, it is finished and I have to reopen it to do some changes. The project is based on STM32L496 microcontroller with x-cube-cellular package. It connects to Azure cloud to send sensors data...

NCatt.1 by Associate III
  • 1396 Views
  • 2 replies
  • 0 kudos

stm32f103c8 canbus problem

stm32f103c8 canbus problemstm32cube version 6.2.1hal version 1.8.3when i want to send data from can bus, , it doesn't work when usart global interrupt is not on, is this error? Is it normal, I couldn't understandusart1 global interrupt=enabled >> w...

HKiri.1 by Associate
  • 681 Views
  • 0 replies
  • 0 kudos

Resolved! I have a project using STM32H745 processor that has network connectivity. All works awesome until the processor temp reaches about 120 F, then I start to lose connectivity. I am using RMII interface and again works perfectly at high bandwidth when < 120F

What could be the cause. I have checked the power circuitry. The rest of application still functions well. DMA, Timers, SPI, etc. Just network data is stalled. When temp goes down it resumes.

DPitt.1 by Associate II
  • 6620 Views
  • 17 replies
  • 0 kudos