STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! USBX on STM32H5 CDC - Can't open port.

Hi. Unfortunately, after several days of struggling with USBX, I'm forced to ask for your help. I'm using custom boards with the STM32h503RB and STM32h563VI. I tested the old library according to forum guides – no response when connected to a PC. The...

Jin454 by Associate III
  • 577 Views
  • 4 replies
  • 0 kudos

Low TCP/IP Data Transfer Rate Using LWIP

Edited by a ST moderator to be comliant with the ST community rules. In next time please use </> button to paste your code. Please review How to insert source code. Hi, I have a video application using F767 with LWIP and without RTOS. The custmized b...

Chao by Senior II
  • 1338 Views
  • 8 replies
  • 3 kudos

Resolved! USBX Audio Class Microphone example

Hi,I've implemented a USBX Audio device correctly using ThreadX and the USBX Middleware on an STM32U5 (working as a speaker).I would like now, to implement a microphone using the same USBX Middleware. For that, I would like to figure out if there are...

nico23 by Senior III
  • 795 Views
  • 4 replies
  • 1 kudos

Resolved! Using UID_BASE to obtain the STM32 96-bit UID

Originally a comment on the How to obtain and use the STM32 96-bit UID Knowledge Base article;Moved for better discussionHello,@MCU Support TD  Can I query the following please (correct me if i'm wrong): "If you are not using HAL, then the CMSIS devi...

###### by Senior II
  • 479 Views
  • 3 replies
  • 5 kudos

Resolved! [STM32H563] NetX Duo slow TLS handshake

Hello!I have an MQTT project using NetX Duo, which publishes MQTT messages to a remote server. But, before it can do that, a secure connection must be established using TLS v1.2, which takes about 18-20 seconds (checked while debugging and stepping t...

Sander_UP by Associate III
  • 880 Views
  • 4 replies
  • 0 kudos