STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

F103C8 USART DMA Issue

Hi, I'm having the following issue with the F103C8 USART DMA.After reset, sometimes the USART DMA Receive doesn't work. It doesn't happen every time, but it happens about once every 10 resets. HAL_UARTEx_ReceiveToIdle_DMA(&huart1, (uint8_t *)RxDataUs...

asttekin by Associate II
  • 309 Views
  • 3 replies
  • 1 kudos

Resolved! Simple ISR for DMA

I'm losing my mind a little, because this seems like it should be a simple task. I have configured my I2C module to enable DMA and interrupts: I can confirm that my call to HAL_I2C_Master_Transmit_DMA returns OK. I can also confirm that the generate...

avidroneg_0-1760975095854.png
avidroneg by Associate III
  • 449 Views
  • 4 replies
  • 3 kudos

Resolved! STM32N6 DK ETH problem

I use STM32Cube FW_N6 V1.2.0 to create an FW to run a web server on the DK board. I figured out that I can not talk to the PHY chip to read the PHY ID. I compared the code with another example that ST released and figured out that these codes are mis...

AliR by Associate
  • 341 Views
  • 2 replies
  • 1 kudos

DMA2D minimum width requirement?

Hello,I'm using a H743 with the DMA2D device in RegToMem mode.  Generally it seems to work for larger images, but I've been trying to fill a small rectangle (5 x 60) pixels, and I was expecting 300 write pulses.  Instead, I'm getting 480 pulses (8 x ...

matt-crc by Senior III
  • 279 Views
  • 2 replies
  • 0 kudos

CAN RX ring buffer interrupt

I am simulating messages to be received via CAN on the STM32F0xx series uC. The hardware FIFO does not overflow as I have activated the overflow interrupt and checked the FIFO level, which never exceeds 1. The current implementation consists of a 128...

Resolved! My STM32 Code only works under debug mode

#include <stdint.h> #include <stdio.h> #include "stm32f4xx.h" volatile uint8_t rxdata = 0; int main(void) { SystemInit(); SystemCoreClockUpdate(); // clock configutation RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB, ENABLE); // TX: PB6 RX: PB7 RCC...

XY by Associate II
  • 778 Views
  • 10 replies
  • 7 kudos