cancel
Showing results for 
Search instead for 
Did you mean: 

STM32N6 DK ETH problem

AliR
Associate

I use STM32Cube FW_N6 V1.2.0 to create an FW to run a web server on the DK board. I figured out that I can not talk to the PHY chip to read the PHY ID. I compared the code with another example that ST released and figured out that these codes are missing on HAL_ETH_MspInit

 

__HAL_RCC_ETH1MAC_CLK_ENABLE();

__HAL_RCC_ETH1RX_CLK_ENABLE();

__HAL_RCC_ETH1TX_CLK_ENABLE();

 

after adding this to my MSPInit function problem was solved!

 

I wonder if this is a bug in this package or if I need to set it in the CubeMX settings?

1 ACCEPTED SOLUTION

Accepted Solutions
STackPointer64
ST Employee

Hello @AliR,

This issue has already been escalated to the relevant team for resolution and is being tracked internally under ticket number 213570. Thank you again!

Best regards,

To improve visibility of answered topics, please click 'Accept as Solution' on the reply that resolved your issue or answered your question.

View solution in original post

2 REPLIES 2
STackPointer64
ST Employee

Hello @AliR, and welcome to ST Community!

Thank you for reporting this. I will investigate this and get back to you with feedback.

Best regards,

To improve visibility of answered topics, please click 'Accept as Solution' on the reply that resolved your issue or answered your question.
STackPointer64
ST Employee

Hello @AliR,

This issue has already been escalated to the relevant team for resolution and is being tracked internally under ticket number 213570. Thank you again!

Best regards,

To improve visibility of answered topics, please click 'Accept as Solution' on the reply that resolved your issue or answered your question.