STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H7B0VBT6: Can I use USB HS at VDD=1.8V?

Hello,We are designing a board with an STM32H7B0VBT6 and USB3320 USB HS-transceiver. The MCU will run at VDD=1.8V. In AN5307, p. 11 it is written:"On some packages neither the VDD33USB pin, nor the VDD50USB pin are available, it is the VDD pin which ...

JWeij.2 by Associate
  • 1502 Views
  • 1 replies
  • 0 kudos

TouchGFX 4.21 + Azure RTOS on STM32F7

Has anyone been able to convert a TouchGFX project from FreeRTOS to Azure RTOS by simply using the freeRTOS compatiblity module provided, then changing the oswrapper files to use non-CMSIS calls (pure FreeRTOS API) and no other changes? This would b...

keymaker by Associate
  • 1377 Views
  • 0 replies
  • 0 kudos

Working with STM32 CDC_RNDIS USB library. Trying to understand the (*Process) function in USBD_CDC_RNDIS_ItfTypeDef

Hi,I'm trying to understand the purpose of CDC_RNDIS_Itf_Process in usbd_cdc_rndis_if_template.c. The @brief for this function is the same as CDC_RNDIS_Itf_Receive function, which I think is incorrect. I can't find any calls to this function ( USB_CD...

HCour.1 by Associate II
  • 2201 Views
  • 3 replies
  • 2 kudos

Enable Ethernet on STM32H743 using ThreadX

Greetings !I am working on STM32H743 and I could able to up Ethernet using LwIP. But I am not able to enable and ping Ethernet with ThreadX (Trying sample TCP echo server application). Requesting procedures / suggestions to achieve the same.Thanks in...

PG.9 by Associate III
  • 1685 Views
  • 1 replies
  • 0 kudos

STM32G0B01xx Dual bank boot implementation

I am missing a description how the dual bank boot is implemented in mentioned devices.From what I found the information is missing in AN2606.Another question is how do I securely detect from which bank my FW is currently running (or rather which bank...

Schue by Associate II
  • 3645 Views
  • 3 replies
  • 0 kudos