STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H745 and RTOS timers

I'm using AzureRTOS to develop on the STM32H745. I've started with the CM7 core and I've generated some basic code using CubeMX. I've selected TIM6 as a time base for HAL, since AzureRTOS will take over systick for it's uses.I've made a couple thre...

Resolved! HAL_I2S_Receive gives 0s although codec transmits data

Hello!For a week i've been trying to configure my stm32f302cbt6 and the tlv320aic3254 codec to trasmit data to the mcu through i2s_ext_sd but HAL_I2S_Receive returns 0s to the buffer although i see data coming out of the codec. I have configured i2s2...

PPats.1 by Associate III
  • 4862 Views
  • 7 replies
  • 0 kudos

Flash Erase on STM32G4 doesn't work as intended

I'm running a STM32G473CB with 128kb flash, and I'm getting some issues erasing pages in bank2 of the flash. Using HAL_FLASHEx_Erase the way it's meant to be used, like in the following code that's supposed to erase pages 30 and 31 of bank2, I don't ...

schwil by Associate II
  • 3798 Views
  • 5 replies
  • 0 kudos

Resolved! STM32G0B USB error during initialization, SOLVED by modifying your library

in usb library in the file generated by STM32CubeMx for the STM32G0B1 * @file          : Target/usbd_conf.c * @version       : v3.0_Cube * @brief         : This file implements the board support package for the USB device libraryin function void HAL_...

GPREV.1 by Associate II
  • 1904 Views
  • 2 replies
  • 2 kudos