STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to receive data from USB peripheral via MAX3421E.

Hi,     I am using STM32 in my project. The use case includes the following :-1) ID accessory(pen drive) ----> STM32.In this STM32 should act as a USB host and detect the ID accessory as well as do some data transfer. We are going to use MAX3421E whi...

Snehal by Associate II
  • 7179 Views
  • 11 replies
  • 1 kudos

Search for a solution on encoding audio in S/PDIF

Hello,I'm looking for a simplest solution for encoding 1 channel audio.Ideally at input - signal from microphone, ADC - not necessary high-end (10...12bit sufficient), output - S/PDIF. Does exist an IC that integrates whole this stuff ?Thanks.

Pavel_47 by Associate III
  • 1342 Views
  • 1 replies
  • 1 kudos

Uart configuration STM32G0

Hi, There is possible to set up USART2 on PA2 and PA15? In documentation in both pins is possible to use USART2 (PA2 as TX and PA15 as RX).I try do it, but I don't get interrupt when data is send to RX pin. On Uart1 (PA9, PA10)  it's work correct. Fo...

arekj by Associate II
  • 2292 Views
  • 2 replies
  • 1 kudos

1. Does STM32U575 support Zephyr RTOS? 2. Does STM32U5A9 support Zephyr RTOS? 3. How can we port the Zephyr to STM32U5A9 if STM32U5A9 doesn't support it?

1. We found that STM32U575 is on the supported list of Zephyr. Does it mean that STM32U575 support Zephyr RTOS?2. We cannot find the STM32U5A9 on the supported list of Zephyr. Does STM32U5A9 support Zephyr RTOS?3. How can we port the Zephyr to STM32U...

VLi.3 by Associate
  • 3192 Views
  • 3 replies
  • 0 kudos

[NUCLEO-H743ZI] USB: How to check the reason of the BROKEN_PIPE(-EPIPE) message from the USB Device?

Hello!HW: NUCLEO-H743ZISW: MxCube v6.8.1Application: USB CDCOS: Ubuntu 20.04.1  5.15.0-75USB Hub: No, the device is connected directly to the USB port (without any USB hubs usage) It was generated a USB CDC Application solution by using MxCube v6.8.1...

usbmon2_v002_dev2-68-1_001.png