STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F4 Another USB Host MSC problem.

Hello, by using a STM32F429I-DISC1 I'm trying to read/write to a thumb drive.When I open and load the provided example in fw packet, it works without problem but that example is an old one and not a CubeMX example so it makes things rough for me.I tr...

RÖztü.1 by Associate II
  • 6144 Views
  • 11 replies
  • 0 kudos

Place const at specific flash location

Hi everyone,I am developing a custom bootloader and before flash the new application image, the bootloader must ensure that the image corresponds to the board, so I think a simple way to do it is to store a specific value (constant uint32_t) into a s...

manuislet by Associate II
  • 3100 Views
  • 4 replies
  • 0 kudos

STM32F446RE Nucleo - USB HOST HID

I followed your videos where the implementation of the USB HOST HID is explained. However, the development board I am using is different from the one shown in all the videos. So the VBUS control circuitry does not exist in the STM32F446RE nucleo docu...

AReal.1 by Associate
  • 2148 Views
  • 2 replies
  • 1 kudos

how to use dual simultaneous adc with DMA

So I Am trying to use the dual regular simultaneous mode with DMA transfer, I tried to use one ADC with the DMA transfer and It works fine but with 2 ADCs I use the function HAL_ADCEx_MultiModeStart_DMA() but the called back function is not actually ...

DEska.1 by Associate II
  • 2800 Views
  • 2 replies
  • 1 kudos

How MAC, FIFO and DMA descriptor is dealing with received frames from and UDP client using HAL libraries?

I have read the datasheet where this part of ethernet is explained. But I have not clear of all taking it to a practical case. Case: Client is sending constantly requests to the stm32f207 HAL based with Lwip stack and no RTOS udp server. Client reque...

genisuvi by Associate III
  • 2911 Views
  • 4 replies
  • 0 kudos