cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H7: New HAL and PBUF_POOL usage

Hi all,

I am developing an application using bare TCP and UDP connections.

Since the new HAL implementation now uses custom PBuf allocation for Rx memories, I thought about killing the PBUF_POOL since it does not seem to be used anymore now.

I started by testing my application with statistics enabled and indeed, the usage count of memp_stats_PBUF_POOL stayed at zero all the time.

Setting PBUF_POOL_SIZE to 0 reduced my RAM usage as expected and the application is still running normally.

Am I missing anything here? Are you guys aware of some pitfall I did not see or do you think I am safe so far?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
MWB_CHa
ST Employee

Probably too late to answer, sorry, but it might help others with same issue:

We can confirm that new HAL Ethernet implementation now uses custom PBuf allocation for Rx and PBUF_POOL is not used anymore in interface and apps.

But PBUF_POOL is used inside LwIP stack. In fact in LwIP\src\core\udp.c line 391 PBUF_POOL is used: 

“q = pbuf_clone(PBUF_RAW, PBUF_POOL, p);�?

In your case, maybe PBUF_POOL is not used by LwIP stack but it can happen in other cases.

So before killing the PBUF_POOL, you have to verify that LwIP stack is not using PBUF_POOL first.

I hope it helps.

View solution in original post

1 REPLY 1
MWB_CHa
ST Employee

Probably too late to answer, sorry, but it might help others with same issue:

We can confirm that new HAL Ethernet implementation now uses custom PBuf allocation for Rx and PBUF_POOL is not used anymore in interface and apps.

But PBUF_POOL is used inside LwIP stack. In fact in LwIP\src\core\udp.c line 391 PBUF_POOL is used: 

“q = pbuf_clone(PBUF_RAW, PBUF_POOL, p);�?

In your case, maybe PBUF_POOL is not used by LwIP stack but it can happen in other cases.

So before killing the PBUF_POOL, you have to verify that LwIP stack is not using PBUF_POOL first.

I hope it helps.