STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32g484 bootloader communication problems

Hello everybody.I have problems with uarts in the my bootloader. In the main program the communication works OK.The client card is stm32g484 based.The first problem:After HAL_NVIC_SystemReset()from main app enter to bootloader and HAL_UART_Transmit()...

RHert.1 by Associate II
  • 3312 Views
  • 5 replies
  • 0 kudos

Resolved! Save text file to SD card with STM32F7508-DK Card

I want to save a text file to the SD card with the STM32F7508-DK Card, but the code gets stuck during the formatting process of the SD card.Can you help me how to solve this problem?The code line is as follows.  /* USER CODE BEGIN Header */ /** ***...

Resolved! bin file is gigantic, hex and elf files are normal, when defining a section of RAM in STM32F765VITx

I'm trying to define a region of RAM for storing debug information that can persist following a reset (DEBUG_RAM). I'd like to put variables in a section (.debug_ram) that are stored in the DEBUG_RAM memory such its usage properly displays in the Bui...

BobbyBeta by Associate III
  • 8626 Views
  • 6 replies
  • 2 kudos

Resolved! Timer3 disable/enable operation

We are using Timer3 to increment a uint64_t counter for serial port operation and need to be able to grab the counter value in the main loop.  //---------------------------------------------------------------- // -------------- Timer 3 -------------...

Capture.JPG

Resolved! x-cube-cryptolib - Adding to application in Keil IDE

Hello, I've to add the x-cube-cryptolib to our application. I added to include path, the file cmox_low_level.c and the library file libSTM32Cryptographic_CM3.a. I get these errors: \Middlewares\ST\STM32_Cryptographic\lib\libSTM32Cryptographic_CM3.a(1...

KauneR by Associate III
  • 7678 Views
  • 16 replies
  • 1 kudos

Bootloader read memory command fails

Posted on June 13, 2017 at 09:14I'm using an STM32F103 and flashing a code into it using the bootloader. I'm successful in writing the code into the MCU, but when I try reading it using the Read Memory command (pg13) [http://www.st.com/content/ccc/r...

Timer help

Hi,i have a STM32F303RC and i have the following problem:With the Pin A2 i want to produce a sequence of 10 pulses.My attempt is to use a PWM TIMER Channel (TIM2 CH3) in one pulse Mode and retrigger it till i have generated my 10 Steps.However, my co...

pedahl by Associate II
  • 2858 Views
  • 5 replies
  • 1 kudos

STM32G030 sometimes not waking up from STOP 1 Mode

Hey everyone, I have developed a circuit board with STM32G030. I use the STOP 1 mode to save power, the device wakes up on a pin change interrupt.Sometimes the current consumption in STOP 1 mode is around 1,2mA higher mode than normal (3uA) but lower...

JakobB by Associate
  • 2541 Views
  • 2 replies
  • 0 kudos