STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Composite Device problem.

HelloI am working a project that implements CDC_ACM and MSC devices in a composite device.Device Manager displays these as USB Serial Device (Com35 , works) and STM Product USB Device (Mass Storage Device). But Disk Drive does not appear in Explorer ...

lubo by Associate
  • 1824 Views
  • 2 replies
  • 0 kudos

Strange screen behavior when audio start

hi,   I'm using STM32H735G-DK. I coded audio output with sine wave while referencing to the example code(\STM32CubeIDE\STM32CubeH7-master\Projects\STM32H735G-DK\Examples\SAI\SAI_AudioPlay). When I start audio, line out could output the sine wave corr...

f-fujii by Associate
  • 994 Views
  • 0 replies
  • 0 kudos

Set Pending PendSV

I am trying to fire the PendSV interrupt from within SysTick. I was trying to use HAL_NVIC_SetPending() but discovered that this function ignores interrupt IDs of 0 or less. I am looking for an alternative.

JoeJoe by Associate II
  • 907 Views
  • 0 replies
  • 0 kudos

Resolved! Inefficient BSP LCD code

After poking around a bit more in the STM32CubeIDE code, I'm seeing a pattern of issues that indicate a serious lack of understanding on the part of the authors of the shipping BSP code. This code was written several years ago, but it is the shipping...

bitbank by Associate II
  • 2504 Views
  • 3 replies
  • 7 kudos

Problems with ST7789 LCD code (MCD Application Team)

Hi All,I'm new to the STM32 community. I've been sharing a lot of my open source imaging code with the Arduino community for the last few years. Much of the code can run within the CubeIDE without modification.My first test was to get my JPEG and GIF...

Screenshot 2024-04-07 at 11.13.42 AM.png
bitbank by Associate II
  • 2589 Views
  • 1 replies
  • 2 kudos

I'm getting HAL_I2C_STATE_BUSY_RX

Hello,I have developed a code in FreeRTOS mode that contains two main tasks. The first one check if I have received an RX buffer on the I2C bus, and the second one manage the data that has been received.However, after receiving the first buffer, I am...

_legacyfs_online_stmicro_images_0693W00000bkVdiQAE.png _legacyfs_online_stmicro_images_0693W00000bkVdJQAU.png _legacyfs_online_stmicro_images_0693W00000bkVd4QAE.png
Mabou.1 by Associate II
  • 8201 Views
  • 15 replies
  • 0 kudos

Resolved! Storing Images in QSPI Flash

Hello,I am using the STM32H747I-DISCO board for prototyping. I was able to load up the "Tutti Frutti" game demo on the board to verify the hardware. In my own application I was able to store a small 320 x 240 image in the internal flash of the STM32H...

STM32H7 -Dead Time Configuration

Hello everyone,   I need your help for configuring PWM dead time, I have configured below configuration but I received dead time as 5uS. I need 200uS dead Time. Could you please help me.     

M_Sukumar_0-1712555514314.png M_Sukumar_1-1712555556276.png M_Sukumar_2-1712555819081.png
M_Sukumar by Associate III
  • 1371 Views
  • 1 replies
  • 0 kudos