cancel
Showing results for 
Search instead for 
Did you mean: 

How to set up clock in STM32CUbe V6.8.1 to 480Mhz for STM32H750XBH6

AAsad.1
Associate II

Hi

I have upgraded my STMCUBE to the latest version of 6.8.1 and am Using STM32H750XBH6 part, when I try to config the CPU clock to 480Mhz, it raises many error flags and would not allow it (also the Resolve clock Issues Button can not fix it), Note my Device is version Y and I could do it easily in 6.6.1 version.

I want to use the stm32cube_fw_h7_v1110 package, so I need to upgrade the CUBE, is there any work around this?

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
AScha.3
Super User

depending on version they set a (new) limit;

+ you set..scale0 ?


_legacyfs_online_stmicro_images_0693W00000bj8SfQAI.png

If you feel a post has answered your question, please click "Accept as Solution".

I thought Y was rated at 400 MHz, and V was 480 MHz

>>is there any work around this?

You could ignore it, and fix the generated code to the speeds you want

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
AAsad.1
Associate II

AScha.a When I choose the PPL the power regulator setting would go away,

Thanks Tesla DeLorean, How Can I do it?