STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

[STM32L5] OpenBootloader UART errors

Hi, I integrated the OpenBootlader for the STM32L552 to my project and it works normally as expected. I'm only using the UART interface and reduced the boot loader project to the minimum.The problem I'm facing is that sometimes the flashing stops, be...

BViet1_0-1716287516447.png
BViet.1 by Associate III
  • 1891 Views
  • 2 replies
  • 0 kudos

Resolved! SPI with DMA and TFT Display ST7735

Dear STM32 communityI am trying to setup the ST7735 Display (ST7735) with SPI and DMA for a faster refresh rate. Without DMA everything works fine. When i setting up DMA nothing is displayed on the Display.My DMA and SPI Settings are:I want to fill t...

Hans345_0-1715755303173.png Hans345_1-1715755330465.png Hans345_2-1715755355614.png Hans345_4-1715756756137.png
Hans345 by Associate
  • 9898 Views
  • 4 replies
  • 0 kudos

DW3300Q STM32 SDK

Hello! I'm a firmware design engineer, and along with my team, we're working on UWB development. We recently received a Qorvo kit (DW3300QDK1) along with the EVB STM32 Nucleo-F429ZI to work with their SDK. However, we couldn't find any documentation ...

bvega by Associate
  • 1535 Views
  • 2 replies
  • 2 kudos

STM32 DMA & UART

Hello im working on a project where im modifying data on STM32 and transmiting it via UART on my other hardware(ESP32).Im having troubles, my best guess is at sending data thought UART. Because of the delays in my code I've implemented DMA which woul...

thatsAbsurd_0-1716224535712.png

Resolved! ADXL345 library development for STM32F407VG-DISC

Hi everyone, I am kinda new at Embedded programming and I wanna ask a question.I am working on a library development of ADXL345 sensor and when I read the datasheet of this sensor here is the information that I got:"An alternate I2C address of 0x53 (...

testbenchmark_0-1715498328928.png

X-Cube-STL

Bonjour,M-Extend est une société basée à Acigné près de Rennes en Bretagne. Nous sommes équipementiers agricoles et nous fabriquons essentiellement des chargeurs frontaux pour les tracteurs. https://m-x.eu/Je travaille au pôle innovation en tant qu'i...

STM32F765VIT6 and ADS131E08 code

Hello All, I hope you are all doing well !I m writing to ask help, I have problem with my STM32f765vit6 and an  ADS131e08 .My the ADS131E08 stops communicating over SPI in continuous mode after a few seconds and block the SPI communication again. But...

Azer by Associate
  • 2202 Views
  • 2 replies
  • 0 kudos

Resolved! f_write fails the 2nd time its called

Board: STM32F411REGreetings,I am trying to make a program where the mcu read an audio file on the SD card, apply a sound filter on it, and write the output to a different file. The program will split the audio file into small chunks and compute them ...