STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32H7, HAL_Deinit() causes core stall

Hi there, I'm fixing the jump function from my custom bootloader to the application, below the code:  static void __inline__ CheckAPPjumpRESET(void) { /*.-.-.| Local variables: |.-.-.*/ u32t uiI = 0; /*.-.-.| Execution: |.-.-.*/ if(GetRESETkey()...

iTTy by Senior
  • 1961 Views
  • 2 replies
  • 0 kudos

Use of "HAL_Delay" after "osThreadCreate"

Hi all,I am working with the Nucleo-L476RG board.I generated a project with CubeMx and enabling FreeRTOS.At this point the project is running fine.I debug the project and all is working.I put a breack point inside the "SysTick_Handler" and this hadle...

0690X000008A7VVQA0.png 0690X000008A7qYQAS.png
Dev1 by Associate II
  • 7211 Views
  • 10 replies
  • 3 kudos

Resolved! Position Independent Code

HelloI am trying to merge USB CDC code into an existing code which is a Keil multi project code. I am using the USB CDC code generated by stm32cubemx for data transmission and reception testing. The multi project is position independent build and whe...

prsh by Associate II
  • 1896 Views
  • 1 replies
  • 1 kudos

Resolved! STM32f429 disc1 board

Can I know what is difference between internal adc of STM32f429 disc1 board and an external 12bit 1MSPS adc.Which adc to use for any application that needs more accuracy whether I should go for external or internal adc.Will internal adc produces any ...

harry123 by Senior II
  • 1156 Views
  • 1 replies
  • 0 kudos

factory-set programming

Hello,I work in a company that uses stm32F031C4T6 and we manufacture 40,000 cards a year with this reference. I was wondering if it would be possible to ask the manufacturer to program the microcontrollers directly in their factories, because for our...

kolia by Associate
  • 1117 Views
  • 1 replies
  • 0 kudos

Resolved! NetX Duo driver & link-down state

Hi All,I am working at project with STM32H7 and NetX Duo. At current version of Ethernet driver from ST (X-CUBE-AZRTOS-H7 v3.0.0) is not handled by any way state when link is disconnected. Link status variable nx_interface_link_up is set at "Enable L...

JDosp.1 by Associate III
  • 6981 Views
  • 8 replies
  • 4 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.