STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H732 I2S Unstable Clocks (Stutter)

I have set up a project in STM32CubeMX. I have setup both I2S1 for Receiving and I2S2 for Transmiting with DMA. After the normal initalization i start receiving from the DMA:       if (HAL_I2S_Transmit_DMA(&hi2s2, (uint16_t*)&output_buffer, 1) != HAL...

Gkatsos by Associate III
  • 6199 Views
  • 13 replies
  • 0 kudos

Resolved! STM32H747xI Watchdog Timer Stop Functionality

The hardware for my project is an Arduino Opta, which utilizes the STM32H747XI dual core processor. We are trying to implement a watchdog timer for our application because the OS occasionally crashes. The start and kick timer functionality works with...

westman by Associate
  • 1494 Views
  • 1 replies
  • 0 kudos

Resolved! I2C with repeated start condition example

HIGot an I2C device connected to my p nucleo wb 55 board. currently no luck communicating.I've been instructed to to use a  repeated start condition in I2C   https://www.i2c-bus.org/repeated-start-condition/Not sure if my current   HAL functions work...

DS4_0-1723014680800.png
DS.4 by Senior II
  • 5164 Views
  • 4 replies
  • 7 kudos

Resolved! REGARDING THREADX on STM32L496ZG-P

HAI , I have STM32L496ZGP nucleo 144 board, I want port threadx on that. I gone through some youtube video , in that in middleware and software packs option they told to select threadx , but in my STM32cubeIDE , threadx option is not there. Only FREE...

HardFault with exceptions c++

Hello ST Community,I'm working on implementing C++ exceptions in my project. My setup includes an STM32H735 board and I'm using FreeRTOS. Here’s a snippet of my code that involves try and catch blocks:   extern "C" void myTaskFunction(void* pvParamet...

HispaEmo_0-1723017523728.png HispaEmo_1-1723017542009.png
HispaEmo by Associate III
  • 1992 Views
  • 1 replies
  • 0 kudos

Resolved! How do I generate spread spectrum PWM?

Hi,I am using a STM32L452RET6. How do I generate spread spectrum PWM on that particular micro?I read somewhere it has a dedicated mode but did not find where.Is there perhaps a library specifically for it?If it does not have a dedicated mode or perip...

Ricko by Senior III
  • 3152 Views
  • 6 replies
  • 4 kudos