STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Плавний пуск перетворювача на STM32G474

Вітаю. Створив DC-DC перетворювач на мікроконтролері G4 серії. У я кості регулятора використовую апаратний FMAC, current mode. Моє питання стосується перерегулювання рівня вихідної напруги при старті перетворювача. На борту маю апаратну кнопку вимкне...

Resolved! Flashing by UART in STM32F411RE

  After more debugging, the jump function works correctly (PC reaches 0x080208xx, SP and RST are valid), but the app never sends any UART message after jump — even with SystemClock_Config() completely commented out and only HAL_Init() + MX_UART_Init(...

STM32F405RGT6: reset command doesn't work after flash operation

求助篇!使用主控芯片STM32F405RGT6 在操作flash后 复位指令不起作用 这是什么问题呢?////////////////////以下是代码段/////////////////////////////*注释以下语句就可以自动复位成功*/Translation:I'm using STM32F405RGT6 microcontroller, the reset command doesn't work after flash operation. What could be the p...

Wu_wu by Associate
  • 143 Views
  • 3 replies
  • 0 kudos

Resolved! CTS signal on USB CDC

To follow up this thread, CTS signal on USB CDC - STMicroelectronics Community I'm experiencing a similar issue. USBser.sys  have some problem 1. Only DTR Break can control alone you can set  DTR is 1  or 0,  but  RTS have change,RTS only change with...

wjandsq by Associate III
  • 559 Views
  • 14 replies
  • 6 kudos