STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! usb host

Posted on February 26, 2017 at 07:10 Hi Everyone, I'm trying to read from the USB keyboard with a custom board STM32F205RCT6 MCU. I am using USB FS host (host only) with HAL library.but it just works with some keyboards! Other keyboards are...

Resolved! Code jumping unexpectedly to 0xfffffffe

Hi, After successful coding, I suddenly stumbled on this error. I'm simply running this code:  HAL_Init(); /* USER CODE BEGIN Init */ /* USER CODE END Init */ /* Configure the system clock */ SystemClock_Config(); /* USER CODE BEGIN Sys...

RBT-ES by Associate III
  • 2357 Views
  • 3 replies
  • 0 kudos

MQTT Client Problem

Hi ,   Recently, I`m using STM32H7 MCU to implement Ethernet Application. I have try TCP Client Echo from example code and it works. Then I want to try with MQTT and it always gets fault. And using mqtt_client_connect function, it will return ERR_RTE...

Resolved! STM32 H573-DK USBX CDC ACM CLASS Stand-Alone

Hello ST Community,I was trying to use USBX with ThreadX and it worked. So far so good. But in our project, we will use FreeRTOS and after some research and getting in touch with some people, I learned that I can not use USBX with FreeRTOS. So they s...

iCenger by Associate
  • 7870 Views
  • 5 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.