2024-09-04 12:24 PM
Referencing attached project files 'H562VGT6.ioc' and 'Project.ioc'
The 'H562VGT6.ioc' file is firmware for an Application
The 'Project.ioc' file is firmware for board Diagnostics
Both projects are for the same model board
The issues is when I flash a new STM32H562 chip for the first time with project 'H562VGT6' the application fails to run even after a power cycle.
Once the STM32H562 is flashed using the diagnostics project and then reflashed using the application code all runs fine
Both projects appear to be configured the same, any thoughts?