2024-09-05 1:01 AM
Hello everyone,
I'm working with an STM32H750B-DK board featuring the STM32H750XB MCU, and it currently has two "MT25QL512ABB8ESF" flash ICs configured in Dual-Mode QSPI.
I would like to switch to using just one flash IC in standard QSPI mode. Could anyone advise on the necessary changes to configure for a single flash setup?
Thanks in advance!
Following is the existing QSPI init code.
static void MX_QUADSPI_Init(void)
{
/* USER CODE BEGIN QUADSPI_Init 0 */
BSP_QSPI_Init_t qspi_initParams;
/* USER CODE END QUADSPI_Init 0 */
/* USER CODE BEGIN QUADSPI_Init 1 */
/* USER CODE END QUADSPI_Init 1 */
/* QUADSPI parameter configuration*/
hqspi.Instance = QUADSPI;
hqspi.Init.ClockPrescaler = 3;
hqspi.Init.FifoThreshold = 1;
hqspi.Init.SampleShifting = QSPI_SAMPLE_SHIFTING_NONE;
hqspi.Init.FlashSize = 26;
hqspi.Init.ChipSelectHighTime = QSPI_CS_HIGH_TIME_4_CYCLE;
hqspi.Init.ClockMode = QSPI_CLOCK_MODE_0;
hqspi.Init.DualFlash = QSPI_DUALFLASH_ENABLE;
if (HAL_QSPI_Init(&hqspi) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN QUADSPI_Init 2 */
qspi_initParams.InterfaceMode = MT25TL01G_QPI_MODE;
qspi_initParams.TransferRate = MT25TL01G_DTR_TRANSFER;
qspi_initParams.DualFlashMode = MT25TL01G_DUALFLASH_ENABLE;
BSP_QSPI_DeInit(0);
if (BSP_QSPI_Init(0, &qspi_initParams) != BSP_ERROR_NONE)
{
Error_Handler();
}
if (BSP_QSPI_EnableMemoryMappedMode(0) != BSP_ERROR_NONE)
{
Error_Handler();
}
/* USER CODE END QUADSPI_Init 2 */
}
2024-09-05 1:45 AM
Hello @ChameeraW ,
For your STM32H750B-DK board, you can follow the example provided in the STM32CubeH7 repository on GitHub. Specifically, you can refer to the QSPI examples for the STM32H743I-EVAL board ( Projects/STM32H743I-EVAL/Examples/QSPI) . Here is the link to the example: QSPI_MemoryMapped
You can use this example as a reference and update it to match your STM32H750B-DK board.
also to better understand the differences between configuring QSPI for dual and single flash setups, you can compare the following two QSPI examples provided by STMicroelectronics: QSPI_MemoryMapped & QSPI_MemoryMappedDual .
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.