STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB HID Mouse+Keyboard

Hi guys,I've a problem and I hope you can help me.my project must acquire a ps2 keyobard and a ps2 mouse and must be see with the usb.This is ioc configuration:  The first step I tested the firmware only acquire a keyboard and works fine. The PC see ...

usbcfg.PNG usbdevice.PNG Cattura.PNG Cattura2.PNG
Maikip92 by Associate
  • 3122 Views
  • 5 replies
  • 1 kudos

Resolved! File size larger than flash size

Hey everyone I have a qn freejoy.hex is 155kb and my stm32c8t6 is only 64kbs and 128kb how did yall get it flashedRefer freejoy and freejoy configurator It gives me an error file size larger than flash size but other people seems to have workaround a...

Resolved! STM32H750B - TouchGFX and Ethernet

Hi Using the following tools: TouchGFX Designer 4.24.0 CubeIDE 1.16.1 and CubeMx 6.11.0   I have attempted to build a system with ethernet capability.   I added the ethernet peripheral, LwIP compiled it without any errors, but the ethernet does not w...

Snag_15592871.png

Resolved! ST-Link Utility, Can not connect to target!

16:19:16 : Can not connect to target!Please select "Connect Under Reset" mode from Target->Settings menu and try again.If you're trying to connect to a low frequency application , please select a lower SWD Frequency mode from Target->Settings menu.16...

zrtn_0-1710845376910.png
zrtn by Associate
  • 12791 Views
  • 5 replies
  • 1 kudos

GrEq audio library

Hello everyone, I am using a STM32H750 with STM32CubeExpansion_Audio_V1.1.1 and I am trying to use the Graphical equalizer library.This is what I've done: I have an aux audio signal that I'm sampling at 96Khz with a DMA's interrupt transfer every 1 m...

FCola.1 by Associate III
  • 2630 Views
  • 5 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.