STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problem with SPI and ADXL345

 Hi, I’m having trouble reading measurements from the ADXL345 using SPI. I’ve attached a picture from the debugger that shows a view of the variables. The SPI is configured as master full duplex, and I’ve included a screenshot showing the SPI configu...

FilipF303RE_0-1731342474048.png FilipF303RE_1-1731342489083.png

Resolved! SPI Triggering GPIO

SEE EDITI am using the STM32H7B3I-DK. I am trying to write my own simple SPI ISR to handle transmitting and receiving of just one byte I have gotten the slave working with my ISR (while master used HAL). I am now implementing on the master and having...

Resolved! SPI Slave Receiving Every Other Byte

I am using STM32H7B3I-DK running a touchgfx application and acting as SPI Master, and Nucleo-H743ZI as SPI Slave. Both are configured in interrupt mode not using HWNSS. The Master is sending 0,1,2,3,4,5,6,7, but the slave is only receiving 0,2,4,6,0,...

STM32G071CBU6 I2C Bootloader Stops Responding

Hi, I have a custom PCB where I am attempting to bootload an STM32G071CBU6 (using an STM32U575). I am using the bootloader while developing for uploading development builds, so it is being used often. The G0 seems to occasionally, randomly, stop resp...

bhaerel_0-1731638215680.png bhaerel_1-1731638272805.png bhaerel_2-1731638431360.png
bhaerel by Associate
  • 1001 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.