STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32 LWIP FreeRTOS

HelloThis is my first post on the forum, always a happy reader in the past and happy STM32 user as well!Now I want to go a bit further then the standard IO and control. I want to implement LWIP + FreeRTOS with a STM32F7. And yes, the fresh generated ...

JDWBE by Associate III
  • 3725 Views
  • 3 replies
  • 6 kudos

Resolved! #define LAN8742A_PHY_ADDRESS

Posted on April 15, 2017 at 13:11This bug has been reported before, but has survived a couple of cube version bumps.STM32CubeMX 4.20.1 and f7_cube 1.6.1in stm32f7xx_hal_conf.h it defines the PHY address incorrectly#define LAN8742A_PHY_ADDRESS       ...

LWIP Using ICache on STM32H723

Dear all,I'm running the LWIP on a STM32H723 processor and need to enable the ICache and DCache within CubeMX. I'm also using DHCP which will only work when both caches are enabled. When I disable the ICache DHCP will timeout? UDP stop working after ...

wh by Associate III
  • 2958 Views
  • 5 replies
  • 1 kudos

HAL_I2C_GetError() reporting error codes

Hello, We have noticed communication errors with STM32 that is working in our device. The device includes STM32 (master) and TI's battery monitor BQ76952 (slave).Using the same device and same software we noticed three situations that occur randomly:...

KGryn.1 by Associate II
  • 8325 Views
  • 10 replies
  • 3 kudos

Is this a HAL IIC bug?

Hi there,I drove 4 SHT4x by STM32G473VE and used the HAL_I2C_Master_Transmit() and HAL_I2C_Master_Receive() to write and read the sensors.Normally, everything is well.However, if Iunplug the sensor;replug the sensor again;(Not the sensor maybe can NO...

Junde_0-1736739151853.png
Junde by Senior III
  • 1349 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.