STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Can't program STM32H745-Disco

Hi,               I'm using STM32H745-Disco kit. facing some issues while testing, Initially able to configure in STM32Cube IDE software, STm32Cube programmer and STM32CubeMX software's tool without any issues. Now working on testing an hall effect s...

Resolved! FDCAN bootloader for STM32H750VB?

I use a STM32H750 chip and I would like to use the emdedded bootloader with the FDCAN1 interface. AN2606 specifies pins PH13 and PH14 for this version. However, the package I use (STM32H750VBT6 LQFP100) doesn't have these pins exported. Does it mean ...

DBign.1 by Associate
  • 4267 Views
  • 7 replies
  • 2 kudos

Voice compressing in STM32L4

I need to compress voice in STM32L4. Here are my requirements:* STM32L4 run at maximum 80 MHz* Voice to be sampled by ADC/DMA* Flash usage for voice compression < 50 kBytes* RAM usage for voice compression < 64 kBytes* Compressed data < 10% of origna...

RFlod.2 by Senior
  • 3529 Views
  • 9 replies
  • 1 kudos

USBX CDC ACM data read bug?

This behavior seems like a bug.I’m using USBX CDC ACM on a H723 nucleo board. I’m trying to work with the blocking nature of the ux_device_class_cdc_acm_read. For my application, I would like to get data as soon as up to 256 characters are received b...

tec683 by Associate III
  • 12928 Views
  • 18 replies
  • 1 kudos

NUCLEO-H7S3L8 USB_HS Clock Reset Timeout

The USB_OTG_HS peripheral keeps timing out on init and hanging the whole program.I have created a STM32 project using the NUCLEO-H7S3L8 board from the new project menu. I have enabled the USB_OTG_HS as device only (but left the middleware disabled) a...

Linduri by Associate II
  • 1934 Views
  • 2 replies
  • 0 kudos

Wait on HAL_GetTick not working

Hi everyone,I'm new to STM32CubeIDE and encountering an issue with my code. It seems to halt at the following loop:  while ((HAL_GetTick() - tickstart) < wait) { } I've attached the .ioc file for reference. Can someone help me identify why the pr...

mkothuri by Associate II
  • 1788 Views
  • 1 replies
  • 0 kudos