2025-01-16 1:24 AM - last edited on 2025-01-16 2:25 AM by Andrew Neil
Hi,
We are trying to interface ST33KTPM2I3WBZA9 with STM32H735IGT3 using I2C communication.We have used following commands and logic for communication.
#define TPM_I2C_ADDRESS 0x2e << 1
#define TPM_REG_ADDR_COMMAND 0x00
uint8_t command_data = 0x80;
uint8_t read_data1;
uint8_t TPM_WriteReadTest(void) {
if (HAL_I2C_Mem_Write(&hi2c4, TPM_I2C_ADDRESS, TPM_REG_ADDR_COMMAND, I2C_MEMADD_SIZE_8BIT, &command_data, sizeof(command_data), HAL_MAX_DELAY) == HAL_OK) {
//HAL_Delay(10);
} else {
return TEST_FAIL;
}
if (HAL_I2C_Mem_Read(&hi2c4, TPM_I2C_ADDRESS, TPM_REG_ADDR_COMMAND, I2C_MEMADD_SIZE_8BIT, &read_data1, sizeof(read_data1), HAL_MAX_DELAY) == HAL_OK) {
if (read_data1 == command_data) {
return TEST_PASS;
} else {
return TEST_FAIL;
}
} else {
return TEST_FAIL;
}
}
Here when initially tested the "HAL_I2C_Mem_Write" function gets passed for around 2 minutes of power on,after that function fails.With further evaluation the "HAL_I2C_Mem_Write" fails in "I2C_RequestMemoryWrite" function in the API below.
/**
* @brief Write an amount of data in blocking mode to a specific memory address
* @PAram hi2c Pointer to a I2C_HandleTypeDef structure that contains
* the configuration information for the specified I2C.
* @PAram DevAddress Target device address: The device 7 bits address value
* in datasheet must be shifted to the left before calling the interface
* @PAram MemAddress Internal memory address
* @PAram MemAddSize Size of internal memory address
* @PAram pData Pointer to data buffer
* @PAram Size Amount of data to be sent
* @PAram Timeout Timeout duration
* @retval HAL status
*/
HAL_StatusTypeDef HAL_I2C_Mem_Write(I2C_HandleTypeDef *hi2c, uint16_t DevAddress, uint16_t MemAddress,
uint16_t MemAddSize, uint8_t *pData, uint16_t Size, uint32_t Timeout)
{
uint32_t tickstart;
/* Check the parameters */
assert_param(IS_I2C_MEMADD_SIZE(MemAddSize));
if (hi2c->State == HAL_I2C_STATE_READY)
{
if ((pData == NULL) || (Size == 0U))
{
hi2c->ErrorCode = HAL_I2C_ERROR_INVALID_PARAM;
return HAL_ERROR;
}
/* Process Locked */
__HAL_LOCK(hi2c);
/* Init tickstart for timeout management*/
tickstart = HAL_GetTick();
if (I2C_WaitOnFlagUntilTimeout(hi2c, I2C_FLAG_BUSY, SET, I2C_TIMEOUT_BUSY, tickstart) != HAL_OK)
{
return HAL_ERROR;
}
hi2c->State = HAL_I2C_STATE_BUSY_TX;
hi2c->Mode = HAL_I2C_MODE_MEM;
hi2c->ErrorCode = HAL_I2C_ERROR_NONE;
/* Prepare transfer parameters */
hi2c->pBuffPtr = pData;
hi2c->XferCount = Size;
hi2c->XferISR = NULL;
/* Send Slave Address and Memory Address */
if (I2C_RequestMemoryWrite(hi2c, DevAddress, MemAddress, MemAddSize, Timeout, tickstart) != HAL_OK)
{
/* Process Unlocked */
__HAL_UNLOCK(hi2c);
return HAL_ERROR;
}
/* Set NBYTES to write and reload if hi2c->XferCount > MAX_NBYTE_SIZE */
if (hi2c->XferCount > MAX_NBYTE_SIZE)
{
hi2c->XferSize = MAX_NBYTE_SIZE;
I2C_TransferConfig(hi2c, DevAddress, (uint8_t)hi2c->XferSize, I2C_RELOAD_MODE, I2C_NO_STARTSTOP);
}
else
{
hi2c->XferSize = hi2c->XferCount;
I2C_TransferConfig(hi2c, DevAddress, (uint8_t)hi2c->XferSize, I2C_AUTOEND_MODE, I2C_NO_STARTSTOP);
}
do
{
/* Wait until TXIS flag is set */
if (I2C_WaitOnTXISFlagUntilTimeout(hi2c, Timeout, tickstart) != HAL_OK)
{
return HAL_ERROR;
}
/* Write data to TXDR */
hi2c->Instance->TXDR = *hi2c->pBuffPtr;
/* Increment Buffer pointer */
hi2c->pBuffPtr++;
hi2c->XferCount--;
hi2c->XferSize--;
if ((hi2c->XferCount != 0U) && (hi2c->XferSize == 0U))
{
/* Wait until TCR flag is set */
if (I2C_WaitOnFlagUntilTimeout(hi2c, I2C_FLAG_TCR, RESET, Timeout, tickstart) != HAL_OK)
{
return HAL_ERROR;
}
if (hi2c->XferCount > MAX_NBYTE_SIZE)
{
hi2c->XferSize = MAX_NBYTE_SIZE;
I2C_TransferConfig(hi2c, DevAddress, (uint8_t)hi2c->XferSize, I2C_RELOAD_MODE,
I2C_NO_STARTSTOP);
}
else
{
hi2c->XferSize = hi2c->XferCount;
I2C_TransferConfig(hi2c, DevAddress, (uint8_t)hi2c->XferSize, I2C_AUTOEND_MODE,
I2C_NO_STARTSTOP);
}
}
} while (hi2c->XferCount > 0U);
/* No need to Check TC flag, with AUTOEND mode the stop is automatically generated */
/* Wait until STOPF flag is reset */
if (I2C_WaitOnSTOPFlagUntilTimeout(hi2c, Timeout, tickstart) != HAL_OK)
{
return HAL_ERROR;
}
/* Clear STOP Flag */
__HAL_I2C_CLEAR_FLAG(hi2c, I2C_FLAG_STOPF);
/* Clear Configuration Register 2 */
I2C_RESET_CR2(hi2c);
hi2c->State = HAL_I2C_STATE_READY;
hi2c->Mode = HAL_I2C_MODE_NONE;
/* Process Unlocked */
__HAL_UNLOCK(hi2c);
return HAL_OK;
}
else
{
return HAL_BUSY;
}
}
What may be the reason,how can we debug it?
2025-01-16 2:39 AM
Please see the Community Guidelines for how to properly post source code:
How to write your question to maximize your chances to find a solution
I've edited your post, but the indentation was already lost.
@SSAIL2023 wrote:We are trying to interface ST33KTPM2I3WBZA9 with STM32H735IGT3 using I2C communication.
Please show your schematics of how you've done that.
@SSAIL2023 wrote:how can we debug it?
The first thing is to discover what's actually going wrong:
As you're using an external hardware interface, the first thing is to use an oscilloscope or logic analyser to see what's actually happening on the wires.
Then use the software debugger and/or add instrumentation to see what the code is doing internally.
Some things to look at:
Some general debugging tips here:
if (HAL_I2C_Mem_Write(&hi2c4, TPM_I2C_ADDRESS, TPM_REG_ADDR_COMMAND, I2C_MEMADD_SIZE_8BIT, &command_data, sizeof(command_data), HAL_MAX_DELAY) == HAL_OK) {
//HAL_Delay(10);
} else {
return TEST_FAIL;
}
2025-01-16 3:45 AM