STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STL Flash test failed

Hello,I'm working to add the STL Library to my existing project, I'm trying to run the function StlSingleTest but it fails (STL_FAILS) executing the STL_SCH_RunFlashTM(&StlFlashStatus) section.micro: STM32F446ZETFlash:Bootloader: 0x08000000 - 0x0800F...

MauroM by Associate
  • 2891 Views
  • 3 replies
  • 0 kudos

Resolved! STM32 FATFS with SPI FLASH

I am trying to interface a SPI flash from Winbond (W25Q64JV) with FATFS.I have no previous experience with FATFS.I initialize FATFS in CubeMX with the option "used-defined" and modified the MAXIMUM and MINIMUM Sector Size to 4096, as it is the smalle...

STM32L432 LPTIM prescaler behaviour

I have a NUCLEO-L432KC that I am trying to configure such that a LPTIM interrupt fires at a set time period in the future. To simplify calculations, the future time is 2048 low frequency clock ticks away (62.5 ms).I can achieve this with relative sim...

JordanY_1-1738124750443.png JordanY_2-1738124998826.png
JordanY by Associate II
  • 5378 Views
  • 8 replies
  • 0 kudos

Resolved! SDIO, USB Mass Storage, and Mac

Hi! I am trying to learn about interfacing with an stm32f405 as a USB Mass Storage Device. My (homemade) development board has an onboard microSD card slot, and so I would like to present the card as my mass storage. I'm running into some problems wi...

sb_st by Senior II
  • 1508 Views
  • 1 replies
  • 0 kudos

Resolved! Circular dependency in HAL driver for STM32H5.

Hi!I have a project that will not compile due to "error: 'HAL_StatusTypeDef' does not name a type".The project uses STM32H563 and includes file stm32h5xx_hal_conf.h.The HAL_RCC_MODULE_ENABLED and HAL_GPIO_MODULE_ENABLED are defined.When looking into ...

Imre by Associate III
  • 1241 Views
  • 1 replies
  • 0 kudos

STM32 FATFS with SPI FLASH

I am trying to interface a SPI flash from Winbond (W25Q64JV) with FATFSI have no previous experience with FATFS.I initialize FATFS in CubeMX with the option "used-defined" and modified the MAXIMUM and MINIMUM Sector Size to 4096, as it is the smalles...