STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

EEPROM emulation - EE_Init() fail - Step 4

Hi, I'm using en.x-cube-eeprom-v7-0-0 on a STM32L476 and I got a problem during my validation phase.I do lot of write on the EEPROM to be sure my code works well (so lot of CleanUp).Actually, on the step 4 of the EE_Init(), I have a EE_WRITE_ERROR on...

Dams_0-1728637523339.png
Dams by Associate III
  • 1723 Views
  • 1 replies
  • 1 kudos

TouchGFX with USB cdc Host

Hello everyone,I am developing firmware for the STM32F7469I discovery board, and I'm utilizing TouchGFX for the GUI aspect of the project. However, I am encountering a problem when enabling USB-FS HOST functionality. The GUI and other peripherals suc...

Usb host with touch gfx

Hi everyone..I am using USB host for communication CDC along with touch GFX for grafix which will use RTOS, The usb is not getting ready after the start state of usb what will be the issue, but when I configure only USB CDC HOST with out touch GFX it...

FMC gives no output for LCD

Hello,Apologies if this is posted in the wrong location. I am trying to control an LCD (ST7789) with my STM32U5G9J-DK2 using FMC. In CubeMX, I configured the NOR Flash/PSRAM/SRAM/ROM/LCD 1 to use NE1 and A0 with 16 bits of data. I also ensured to con...